Press Release Details

View all news

Avnet to Distribute ACEINNA’s Newest MCx2101 Family of Products

04/15/2024

High-performance current sensors for next-generation automotive power conversion systems

 

PHOENIX – Design engineers will soon have access to ACEINNA’s* new MCx2101 family of AEC-Q100 qualified automotive current sensors via Avnet’s global distribution network. These fully integrated, single-chip solutions offer exceptional accuracy, high bandwidth, and fast response time, making them ideal for demanding automotive power conversion applications in electric, hybrid, and ICE vehicles.

ACEINNA is a leading developer of high performance, thin film Magneto-Resistance (xMR) based current sensors.

“The MCx2101 family pushes the boundaries of current sensor performance, enabling automotive engineers to maximize the benefits of fast switching SiC/GaN power devices and simplify system design and improve overall efficiency. xMR technology represents an advanced technology platform outperforming traditional Hall-based current sensing solutions in bandwidth, response time and noise,” said Teoman Ustun, VP of Automotive Business Unit at ACEINNA. “With industry-leading accuracy, high bandwidth, and fast response time, these sensors contribute to improved performance, protection and reliability across a wide range of automotive power applications.”

“Avnet is pleased to bring ACEINNA’s cutting-edge sensor technologies to market,” said Jason Skoczen, sales director Lightspeed and Transportation, Avnet.  “The MCx2101 family is ideal for the transportation vertical and will allow design engineers to bring higher levels of system efficiencies and integration to their designs.”

Key Features of the MCx2101 Family of Current Sensors:

  • AEC-Q100 qualified for automotive applications
  • Fully integrated single-chip design in SOIC16 package
  • High 3dB bandwidth of 5MHz for fast switching SiC/GaN
  • Low phase delay for fast and stable power control  
  • Fast output response time of 80ns for optimum protection
  • High accuracy with typical total error as low as 0.6%
  • Low noise density of 35 µA/ÖHz for high SNR
  • High PSRR of -80dB @1kHz
  • Operates at 3.3V and 5V for system flexibility
  • Available in fixed gain (MCA) and ratiometric (MCR) options
  • Nominal current ranges from +/-5A to +/-65A
  • Temperature range of -40C to +125C
  • Cost-optimized for volume applications

Target Applications:

  • On-board chargers and fast DC chargers
  • Automotive motor drivers, inverters and servo drives
  • Automotive DC-DC, AC-DC power supplies
  • Solar panel inverters
  • Data center power supplies
  • Uninterruptible power supplies (UPS)
  • AC-DC Power systems (PFC)

Availability:

For information on ordering the MCx2101 family please visit: MCx2101 | Avnet Americas.

Datasheets and additional product information can be found at https://aceinna.com/current-sensors.

About ACEINNA:

ACEINNA, Inc. is a leading MEMS based sensing solutions company, focusing on the development of innovative Inertial Measurement Unit (IMU) and current sensing technologies that are essential to next generation cars, robots and other autonomous applications. ACEINNA product lines cover high bandwidth, low noise Magneto-Resistance (MR) based electric current sensors, high-performance open source IMUs, Real Time Kinematic (RTK) navigation systems, and centimeter-precision positioning services. ACEINNA is committed to providing exceptional customer service and support, and is recognized as a trusted partner by leading companies around the world.

 

About Avnet

As a leading global technology distributor and solutions provider, Avnet has served customers’ evolving needs for more than a century. We support customers at each stage of a product’s lifecycle, from idea to design and from prototype to production. Our unique position at the center of the technology value chain enables us to accelerate the design and supply stages of product development so customers can realize revenue faster. Decade after decade, Avnet helps its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com. 

 

Follow Avnet on Instagram: http://www.instagram.com/Avnet

Connect with Avnet on Facebook: http://www.facebook.com/AvnetInc

Connect with Avnet on LinkedIn: http://www.linkedin.com/company/avnet

 

 

*Trademarks and brands are the property of their respective owners.

 

Avnet Media Contacts

Jeanne Forbis

Avnet

Jeanne.forbis@avnet.com

480-643-7499

 

ACEINNA Inc., 3 Highwood Dr Suite 101W, Tewksbury, MA 01876
Tel: 978-965-3200 Fax: 978-965-3201

Email: info@aceinna.com 

Web: www.aceinna.com

 

 

Multimedia Files:

View all news