Press Release Details

View all news

Avnet Releases AUBoard 15P Development Kit

05/07/2024

Enables easy creation of complex designs requiring flexibility, speed and parallel processing capabilities

 

PHOENIX – Avnet (Nasdaq: AVT) rolls out a new development kit enabling design engineers to create a spectrum of simple to sophisticated Field Programmable Gate Array (FPGA) applications.

 

The Avnet AUBoard 15P development board features the AMD Artix™ UltraScale+™ FPGA. This FPGA provides the highest serial bandwidth and signal compute density in a cost-optimized device for critical networking applications, vision and video processing, and secured connectivity.

 

By leveraging the capabilities of the abundant GTH multi-gigabit transceivers included in the Artix UltraScale + FPGA, system architects can easily create complex designs that require flexibility, speed and parallel processing capabilities. The board’s SFP+, HDMI 2.0-compatible input and output ports, and 4-lane PCI Express Gen 4 interfaces enable high-speed connectivity, 4K high-resolution video processing, and high-performance computing applications.

 

“The new AUBoard 15P development kit will allow developers to rapidly prototype a wide range of FPGA designs,” said Evan Leal, director, AECG Product Marketing, AMD. “The kit is powered by the AMD Artix UltraScale+ AU15P device, built on the production-proven 16nm architecture, with 170k programmable logic cells and 12 GTH transceivers at 16Gbps supporting a range of onboard functionality. The enhanced connectivity and flexibility enabled by this platform provide engineers with an ideal starting point for the development of applications such as machine vision frame grabbers, medical imaging acquisition and processing, or industrial networking.”  

 

Avnet Vice President of Advanced Applications Jim Beneke said the board provides design engineers an innovative and cost-effective way to bring designs to market faster.

 

“From the abundant logic resources to the numerous high-speed serial interfaces, the AUBoard can help accelerate product development and prototyping, or serve as a production-ready PCI Express endpoint plug-in card,” Beneke said.

 

This product is ideally suited for the following applications:

  • Edge computing
  • Embedded systems
  • Embedded vision
  • Machine vision
  • Industrial networking
  • Industrial automation
  • Medical
  • AV Broadcasting

 

 

The Avnet AUBoard 15P Dev Board is available for pre-order with shipping anticipated in the third quarter of 2024. For more information visit: https://bit.ly/3wi1YoM

For more information on AMD AU+ visit: https://www.xilinx.com/products/silicon-devices/fpga/artix-ultrascale-plus.html

 

 

About Avnet

As a leading global technology distributor and solutions provider, Avnet has served customers’ evolving needs for more than a century. We support customers at each stage of a product’s lifecycle, from idea to design and from prototype to production. Our unique position at the center of the technology value chain enables us to accelerate the design and supply stages of product development so customers can realize revenue faster. Decade after decade, Avnet helps its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com. 

 

Follow Avnet on Instagram: http://www.instagram.com/Avnet

Connect with Avnet on Facebook: http://www.facebook.com/AvnetInc

Connect with Avnet on LinkedIn: http://www.linkedin.com/company/avnet

 

 

Trademarks and brands are the property of their respective owners.

 

Avnet Media Contacts

Jeanne Forbis

Avnet

Jeanne.forbis@avnet.com

480-643-7499

 

Lauren Levinson

Brodeur Partners, for Avnet

llevinson@brodeur.com

202-899-4639

 

 

 

Multimedia Files:

View all news