Press Release Details

View all news

Avnet Launches MaaXBoard OSM93 Development Kit for Design Engineers Seeking an Energy-efficient, Edge AI Single-Board Computer

03/25/2024

Kit will be featured at Embedded World April 9-11

 

PHOENIX – March 25, 2024 – The new MaaXBoard OSM93 development kit from Avnet is the latest single-board computer (SBC) to be added to the popular MaaxBoard series of SBCs based on the i.MX 8 and i.MX 9 series of NXP Semiconductors* application processors. This SBC is ideal for applications targeting building control and automation, EV charging, industrial HMI, industrial gateways, and much more.

The MaaXBoard OSM93 is designed around a production-ready, industry standard OSM (Size-S) solder-down module, which features the i.MX 93 applications processor from NXP. Developers can use the MaaXBoard as a prototyping and development platform for the OSM, or as a production-ready SBC to reduce hardware development time and speed time to market.

“The MaaXBoard OSM93 Development Kit is a great way for embedded designers to quickly evaluate and prototype both the i.MX 93 applications processor from NXP and the Avnet Embedded OSM-SF-IMX93 OSM,” said Jim Beneke, vice president Advanced Applications Group, Avnet. “Targeting high-volume applications, the OSM 1.1 standard module is ideal for low-cost automated assembly, while lower volume applications can make use of the production ready SBC form-factor the MaaXBoard offers.”

“The NXP i.MX 93 applications processor and PCA9451 PMIC are excellent for implementing energy efficient, secure edge-AI applications,” said Amanda McGregor, Senior Director of Product Innovation, Advanced Edge Processing, NXP. “Both the MaaXBoard OSM93 SBC and OSM-SF-IMX93 OSM solder-down SOM provide developers with a range of options to accelerate their prototyping, production, and software development efforts around NXP’s i.MX 93 applications processor."


Kit Features

 

Included on the OSM module is the NXP i.MX 93 applications processor, with dual Arm* Cortex*-A55 cores, an Arm Cortex-M33 core, and an Arm Ethos*-U65 NPU. There is also abundant memory with 2 GB LPDDR4 SDRAM, 16 GB eMMC 5.1 Flash and 16 MB QSPI NOR Flash. The OSM is soldered onto the main SBC carrier board, which provides additional interfaces for three USB 2.0 ports, dual 1 Gbps Ethernet, MIPI-DSI, MIPI-CSI, and a standard 40-pin header with UART, SPI, I2C, I2S, and GPIO connections. The carrier also includes interfaces for JTAG, debug, ADC, CAN-FD, SAI digital audio, two PDM microphones, and an M.2 connector that can support connection to WiFi/BT.802.15.4 wireless modules.

 

The MaaXBoard OSM93 Development Kit includes a downloadable Yocto-based board support package (BSP) along with a number of example designs to help developers get started. Avnet also offers several optional accessories for the MaaXBoard family, including a 7-inch MIPI-DSI LCD touch panel and a 5V/3A (USB-C connector) power supply.

 

See at embedded world in April

This board will be exhibited in the Avnet Embedded booth (Hall 1–510) at embedded world (April 9-11 in Nuremberg, Germany), alongside a range of new development boards engineered by Avnet Embedded, focused on edge-AI applications.

The MaaXBoard OSM93 (AES-MAAXB-OSM93-DK-G) and the i.MX 93 OSM (OSM-SF-IMX93) will be available in Q2 2024. For more information and the option to be notified on pricing and availability, please visit: www.avnet.me/MaaXBoard-OSM93.

 

About Avnet

As a leading global technology distributor and solutions provider, Avnet has served customers’ evolving needs for more than a century. We support customers at each stage of a product’s lifecycle, from idea to design and from prototype to production. Our unique position at the center of the technology value chain enables us to accelerate the design and supply stages of product development so customers can realize revenue faster. Decade after decade, Avnet helps its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com. 

 

Follow Avnet on Instagram: http://www.instagram.com/Avnet

Connect with Avnet on Facebook: http://www.facebook.com/AvnetInc

Connect with Avnet on LinkedIn: http://www.linkedin.com/company/avnet

 

 

*Trademarks and brands are the property of their respective owners.

 

Avnet Media Contacts

Jeanne Forbis

Avnet

Jeanne.forbis@avnet.com

480-643-7499

 

Lauren Levinson

Brodeur Partners, for Avnet

llevinson@brodeur.com

202-899-4639

 

Multimedia Files:

View all news