Press Release Details

View all news

Extend the Lifecycle of C6C-RYZ Modules with New Drop-In Replacement

09/19/2023

New module ideal for medical equipment, digital signage, HMI and automation

 

 

PHOENIX – Design engineers and system architects can now effectively extend the operational lifespan of their previous generation AMD Ryzen™-powered C6C-RYZ COM Express® module with Avnet’s (Nasdaq: AVT) latest module called the MSC C6C-RYZ2. This module builds upon the previous generation, allowing enhanced performance, additional functionality, and prolonged usability.

 

“As a seamless drop-in replacement for the previous generation board, this new module allows designers to easily migrate their application to the new platform,” said Tim Jensen, senior director Embedded Product Innovation, Avnet. “We want to support our customers’ needs throughout the entire lifecycle of their products and this module enables both a performance upgrade and adds at least four years to the application lifecycle.”

 

The MSC C6C-RYZ2 module is the embedded platform for the AMD Ryzen Embedded R2000 processor family. This versatile system-on-chip (SoC) technology combines processing, graphics and I/O functionality on a single die, allowing for outstanding compute performance in environments with constrained real estate, power and cooling. Designers can choose a variety of quad and dual-core processors to scale performance and capabilities according to application requirements.

 

This module is ideal for medical equipment (e.g. eye surgery, ultrasound), digital signage, HMI (human machine interface), and automation.

 

Features

 

  • Scalable and power efficient platform for compute and graphics intensive applications
  • Compact product providing high processing and graphics performance
  • Four independent graphic streams
  • Rich I/O including Display Ports, eDP, LVDS, USB 3.2, USB 2.0

 

The board provides support for up to four independent displays with up to 4k x 2k resolution, highest level graphics acceleration and hardware-based video en-/decoding. Fast DDR4 memory and multiple USB 3.2/2.0 interfaces complete the compact and power saving module.

 

The MSC C6C-RYZ2 offers hardware-based security compliant to the requirements of TCG (Trusted Computing Group) and features TPM 2.0 capability.

 

The Type 6 pin-out allows direct access to the latest digital display interfaces like DisplayPort, HDMI 2.0b and DVI as well as up to four USB 3.2 interfaces.

 

The MSC C6C-RYZ2 is available for orders now. For more information, please visit https://embedded.avnet.com/com-express

 

 

About Avnet

As a leading global technology distributor and solutions provider, Avnet has served customers’ evolving needs for an entire century. We support customers at each stage of a product’s lifecycle, from idea to design and from prototype to production. Our unique position at the center of the technology value chain enables us to accelerate the design and supply stages of product development so customers can realize revenue faster. Decade after decade, Avnet helps its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at avnet.com.

Follow Avnet on Twitter: @Avnet

Follow Avnet on Instagram: http://www.instagram.com/Avnet

Connect with Avnet on Facebook: http://www.facebook.com/AvnetInc

Connect with Avnet on LinkedIn: http://www.linkedin.com/company/avnet

 

All brands and trade names are trademarks or registered trademarks and are the properties of their respective owners. Avnet disclaims any proprietary interest in marks other than its own.

 

 

Media Contact

Jeanne Forbis

Avnet

jeanne.forbis@avnet.com

480-643-7499

 

Alex Wood

Avnet

Alex.wood@avnet.com

 

Multimedia Files:

View all news