Skip to main content

Press Release Details

View all news

Avnet and Fujikura Accelerate 5G mmWave Phased Array Antenna-to-Bits System Design with 5G mmWave PAAM Development Platform

05/25/2023

PHOENIX – Avnet, Inc. (Nasdaq: AVT) and Fujikura released their 5G FR2 phased array antenna development platform for mmWave frequency bands. This platform enables customers to quickly develop and prototype advanced 5G mmWave systems using AMD ZynqTM UltraScale+™ RFSoC Gen3 and Fujikura’s FutureAccess™ Phased Array Antenna Module (PAAM), controlled by the Avnet RFSoC Explorer® MATLAB dashboard. This combination of leading-edge RF system-on-chip, mmwave beamforming array, and intuitive software allows customers to quickly prototype with Fujikura’s compact PAAM and AMD RFSoC architecture. It is available for order now.

“With the acceleration of the 5G market, higher bandwidth applications are driving the need for mmWave technology, especially in the industrial and telecom segments,” said Jim Beneke, vice president of Advanced Applications Group, Avnet. “Through our collaboration with Fujikura, AMD and MathWorks, we’re announcing our new platform that brings together the key building blocks of mmWave radio solutions allowing designers to quickly prototype communications algorithms, reduce engineering time, and get into the 5G market even faster.”

The addition of the easy-to-use Avnet RFSoC Explorer MATLAB application enables smoother development and prototyping of advanced 5G mmWave systems using AMD’s RFSoC Gen3 and Fujikura’s 5G PAAM. Not only can it be extended to control the entire system from antenna to digital, but it also enables customers to implement and test mmWave beamforming applications quickly without HDL or software coding.

“Our collaboration on the Avnet RFSoC Explorer MATLAB app demonstrates how 5G standard waveform generation combined with signal analysis capabilities can help engineers get their wireless designs completed faster,” said Noam Levine, partner manager at MathWorks. “MathWorks and Avnet have enjoyed over a decade of working together on wireless and mmWave applications, and we look forward to working with them and Fujikura on this latest PAAM Development Platform.”

The Fujikura PAAM operates in the 3GPP FR2 frequency bands n257 (28 GHz), n258 (26 GHz), and n261 (27 GHZ) allowing for use in both indoor and outdoor applications. It is a complete PAAM module with a highly integrated 8x8 antenna element, RF ICs, filter, and optimal TCO. This high level of integration enables compact product design and quick time to market. With high-power efficiency and extremely fast beam switching (<220ns), Fujikura PAAM based systems can obtain industry leading performance. Also, with a calibration free architecture and Fujikura’s extreme attention to quality, end customers will have a significant advantage in system integration, manufacturing, deployment and longevity.

 

“Fujikura is committed to 5G mmWave technology which substantially expands the 5G value proposition. Significant 5G mmWave growth is being seen in Fujikura targeted areas of Fixed Wireless Access (FWA), mobile broadband, and high-density indoor coverage systems in venues such as stadiums and shopping malls.” said Dr. Kobayashi, head of Electronic Technologies R&D Center at Fujikura. “We are excited to partner with Avnet, a global leader in technology distribution, and bring Fujikura’s innovative PAAM solutions to a worldwide customer base via this collaboration.”

 

The Avnet-Fujikura 5G mmWave PAAM Development Platform will be demonstrated at the Avnet-Fujikura IMS Conference Booth #2514 in San Diego, June 13-15. It will also be used during the IMS Workshop, “Validating a CATR Benchtop OTA Test System for 5G FR2 Phased Array Antenna R&D Testing.”

The Avnet-Fujikura 5G mmWave PAAM Development Platform is available for orders now. For more information on the product and pricing please visit: avnet.me/5g-mmwave-paam-platform   

 

About Fujikura

Fujikura has been providing highly reliable products and services in the four business fields of energy, information and communications, electronics, and automotive electrical equipment since its establishment in 1885. Currently, this company is working in the mmWave wireless communication field as its new business. The company is developing 5G mmWave devices for both licensed and unlicensed bands, making full use of its proprietary technologies of phased array antenna design, flexible printed circuit board manufacturing, and electromagnetic field analysis. For more information, visit the Fujikura company website: https://www.fujikura.co.jp/eng/ or the product website: https://mmwavetech.fujikura.jp/5g/.

 

About Avnet

As a leading global technology distributor and solutions provider, Avnet has served customers’ evolving needs for an entire century. We support customers at each stage of a product’s lifecycle, from idea to design and from prototype to production. Our unique position at the center of the technology value chain enables us to accelerate the design and supply stages of product development so customers can realize revenue faster. Decade after decade, Avnet helps its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at avnet.com.

Follow Avnet on Twitter: @Avnet

Follow Avnet on Instagram: http://www.instagram.com/Avnet

Connect with Avnet on Facebook: http://www.facebook.com/AvnetInc

Connect with Avnet on LinkedIn: http://www.linkedin.com/company/avnet

 

All brands and trade names are trademarks or registered trademarks and are the properties of their respective owners. Avnet disclaims any proprietary interest in marks other than its own.

 

 

Media Contacts

Jeanne Forbis

Avnet

jeanne.forbis@avnet.com

480-643-7499

 

Lauren Levinson

Brodeur Partners, for Avnet

llevinson@brodeur.com

202-899-4639

Multimedia Files:

View all news