STUTENSEE, GERMANY – Avnet Embedded presents the compact MSC OSM-SF-IMX93 OSM computing modules compliant with the new OSM* 1.1 standard (Size-S) “Small” with dimensions of 30 x 30mm. The scalable standard module family integrates i.MX 93 applications processors from NXP* Semiconductors.
The MSC OSM-SF-IMX93 OSM modules housed in a pre-tinned LGA package can be soldered directly to the PCB and are suited for fully automated soldering, assembly and testing processing. By reducing the number of production steps and eliminating the cost of a connector, significant cost savings can be achieved compared to existing module form factors. The solder-on modules are optimized for large quantities.
The compact MSC OSM-SF-IMX93 module family is mainly used in industrial low-power applications that are cost-sensitive or need small dimensions. Typical examples include optimized IoT systems such as small gateways, industrial control systems and home automation solutions. The OSM boards are particularly rugged and resistant to shock and vibration and are specified for the extended temperature range from -40 to +85 °C.
Tim Jensen, Director of Product Innovation, Avnet Embedded, said: ”The compact, scalable OSM embedded computing modules are optimized for large quantities and open numerous innovative application fields.”
Avnet Embedded develops all embedded modules in its company-owned design centers. The products are manufactured in large quantities in highly automated production facilities in Germany. Avnet Embedded’s first OSM products MSC OSM-MF-IMX8MINI and MSC OSM-MF-IMX8NANO are based on NXP Semiconductors’ i.MX 8M Mini and i.MX 8M Nano SOCs with Arm® Cortex™-A53 processors.
Technical specifications:
Avnet Embedded’s compact MSC OSM-SF-IMX93 OSM module family is highly scalable and equipped with i.MX 93 applications processors manufactured by NXP Semiconductors. The processors integrate single or dual Arm Cortex-A55 cores up to 1.7GHz bringing performance and energy efficiency to Linux-based edge applications. The Arm Ethos*-U65 microNPU enables developers to create capable, cost-effective and energy-efficient machine learning (ML) applications. The i.MX 93 processors deliver advanced security with integrated EdgeLock secure enclave and an efficient 2D graphics processing unit (GPU).
The MSC OSM-SF-IMX93 modules provide fast and low power LPDDR4 memory technology with inline ECC support, combined with up to 256GB eMMC Flash memory. Various interfaces for embedded applications such as Dual Gigabit Ethernet (RGMII), USB 2.0, 2x CAN-FD, MIPI-DSI and MIPI CSI-2 (2-lane) for connecting a camera are available. The typical design power ranges from 2 to 4W.
For evaluation and design-in of the new MSC OSM-SF-IMX93 modules, Avnet Embedded provides a development platform, a starter kit and comprehensive design services. A Yocto based Linux Board Support Package is available (Android support on request).
For more information, please visit: https://embedded.avnet.com/product/msc-osm-sf-imx93/
*All brands and trade names are trademarks or registered trademarks, and are the properties of their respective owners. Avnet disclaims any proprietary interest in marks other than its own.
About Avnet Embedded
Avnet Embedded builds embedded compute, display and software solutions that meet the demand for innovation and quality, with reduced time to market, utilizing Avnet Embedded’s platform technologies, design and manufacturing capabilities, and a world-class team of experts.
From luxury kitchen appliances to industrial farming equipment, Avnet Embedded helps its customers to build the best products for their market. Some of the world’s most well-recognized industry leaders trust Avnet Embedded as their partner, to get their products to market faster, better and stronger.
About Avnet
As a leading global technology distributor and solutions provider, Avnet has served customers’ evolving needs for an entire century. We support customers at each stage of a product’s lifecycle, from idea to design and from prototype to production. Our unique position at the center of the technology value chain enables us to accelerate the design and supply stages of product development so customers can realize revenue faster. Decade after decade, Avnet helps its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at avnet.com.
Follow Avnet on Twitter: @Avnet
Follow Avnet on Instagram: http://www.instagram.com/Avnet
Connect with Avnet on Facebook: http://www.facebook.com/AvnetInc
Connect with Avnet on LinkedIn: http://www.linkedin.com/company/avnet
All brands and trade names are trademarks or registered trademarks and are the properties of their respective owners. Avnet disclaims any proprietary interest in marks other than its own.
Media Contacts
Jeanne Forbis
Avnet
jeanne.forbis@avnet.com
480-643-7499
Alex Wood
Avnet
Alex.wood@avnet.com