Press Release Details

View all news

Avnet Launches ZUBoard Development Kit based on the Newest AMD-Xilinx Zynq UltraScale+ MPSoC Device

05/11/2022

See special preview of board at Embedded Vision Summit May 17-19

in Santa Clara, Calif.

 

PHOENIX – The new Avnet development kit called the ZUBoard 1CG, based on the newest member of the AMD-Xilinx Zynq UltraScale+ MPSoC family, will be on display at the Embedded Vision Summit being held May 17-19, 2022 in Santa Clara, Calif. This kit features the lowest cost member of the AMD-Xilinx Zynq UltraScale+ MPSoC, enabling engineers to jump-start their design work.

The kit will enable engineers to learn the basics of the Zynq UltraScale+ MPSoC architecture and the Vivado ML and Vitis development environments. Experienced engineers can design complex prototypes for artificial intelligence and machine learning, adding any necessary hardware through the SYZYGY and Click Board interfaces.

The board features three SYZYGY sites, one Click Board site and 45W of input power, exposing 87 free I/O and four PS GTR transceivers. This allows for extensive proof-of-concept opportunities through add-on boards. Example designs and a Linux board support package (BSP) are provided to accelerate an engineer’s design. In addition, complex circuit and layout examples for Zynq UltraScale+ MPSoC power, LPDDR4, Ethernet and USB design are also provided.

The kit will allow developers to evaluate some of the key features of the Zynq UltraScale+MPSoC device, including the powerful Arm® Cortex®-A53 and Arm Cortex-R5F based processing subsystem for analytics and complex decision making, the on-chip memory which helps eliminate system performance bottlenecks, the DSP blocks for offloading compute intensive applications and the ample programmable fabric with 81K system logic cells enabling adaptable hardware for an assortment of additional functions.

“We are excited to be collaborating with Avnet on their ZUBoard 1CG Development Kit featuring our Zynq UltraScale+ ZU1CG device – the smallest, lowest power, and most cost-optimized member of the Zynq UltraScale+ family,” said Evan Leal, director of Product Marketing for Cost Optimized Silicon products at AMD-Xilinx. “This kit will give any developer a jump-start towards building their own ZU1CG MPSoC-based end systems like miniaturized, compute-intensive edge applications in industrial and healthcare IoT systems, embedded vision cameras, AV-over-IP 4K and 8K-ready streaming, hand-held test equipment, consumer, medical applications and more.”

“This board is ideal for design engineers, software engineers, system architects, hobbyists, makers and even students,” said Bryan Fletcher, technical marketing director, Avnet. “We have provided an advanced and affordable example design with the AMD-Xilinx Zynq Ultrascale+ MPSoC, along with 20+ other Avnet suppliers represented on the board.”

Developers can get up to speed quickly on Zynq UltraScale+ MPSoC design by using Avnet’s provided resources to learn several example designs. Avnet’s field resources can also help them utilize this design in their custom developments, helping them avoid common design errors and costly board turns. The board is available for $159 and can be pre-ordered with shipping estimated in Q4 of 2022. For more information visit: www.avnet.me/zuboard-1cg

 

About Avnet

As a leading global technology distributor and solutions provider, Avnet has served customers’ evolving needs for more than a century. We support customers at each stage of a product’s lifecycle, from idea to design and from prototype to production. Our unique position at the center of the technology value chain enables us to accelerate the design and supply stages of product development so customers can realize revenue faster. Decade after decade, Avnet helps its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com. 

 

Trademarks and brands are the property of their respective owners.

 

Avnet Media Contacts

Jeanne Forbis

Avnet

Jeanne.forbis@avnet.com

480-643-7499

 

Alex Jafarzadeh

Brodeur Partners, for Avnet

ajafarzadeh@brodeur.com

617-587-2846

 

 

Multimedia Files:

View all news