Press Release Details

View all news

Avnet Launches MaaXBoard 8ULP Starter Kit for Design Engineers Creating Secure Intelligent Edge Applications

06/16/2022

Kit will demo at Embedded World June 21-23

 

PHOENIX – The new MaaXBoard 8ULP starter kit from Avnet features the i.MX 8ULP processor from NXP® Semiconductor and will help facilitate the development of ultra-low power, secure, intelligent edge applications. Implemented as a compact System-on-Module (SOM) plus carrier board (in popular single-board computer format), this platform includes a multifunction development interface plus well supported communication and expansion interfaces, to maximize its overall utility for developers of new custom products.

This board will be exhibited in the Avnet Silica booth at Embedded World (June 21–23 in Nuremberg, Germany), alongside a range of new development boards engineered by Avnet, focused on edge-AI applications.

“Use of the NXP i.MX 8ULP applications processor and PCA9460 PMIC on the Avnet SOM provides a promising new option for developers implementing energy efficient, secure edge-AI applications with advanced audio and display capabilities,” said Amanda McGregor, senior director of Product Innovation, Advance Edge Processors, NXP.

Efficient control of energy usage is facilitated by architectural features of the i.MX 8ULP device, which includes the partitioning of processing resources into application domain (Dual-Core Arm® Cortex®-A55 cores), real-time domain (Arm® Cortex®-M33 core and Fusion DSP), and Low Power Audio Video domain (HiFi 4 DSP).

The MaaXBoard 8ULP’s small, 43mm x 36mm formfactor SOM includes the NXP i.MX 8ULP applications processor and power management IC (PMIC) plus abundant memory resources including:

  • On-chip shared RAM (768 KB)
  • Power-efficient 32bit wide LPDDR4X DRAM (2GB)
  • Octal PSRAM (8 MB)
  • eMMC 5.1 flash (32 GB)
  • Octal SPI NOR flash (4 MB) non-volatile memory

The memory architecture enables ultra-low power capabilities through the support of independent real-time and application processing domains. Two 100-pin connectors interface the SOM to the carrier board.

“Utilizing the small form factor of the MaaXBoard 8ULP ensures the most complex aspects of the hardware implementation are already pre-engineered in the SOM—significantly reducing the engineering risk and providing a path from development to integration into custom products,” said Jim Beneke, vice president of Products & Emerging Technologies, Avnet. “It also reduces supply chain risks, since the compact SOM replaces dozens of components, many of which have long lead times.”

The MaaXBoard 8ULP carrier baseboard (based on compact Raspberry Pi form-factor) supports a versatile set of I/O interfaces. These include:

  • Gigabit Ethernet
  • Two USB 2.0 host interfaces plus USB 2.0 device interface
  • MIPI DSI display and MIPI CSI camera interfaces
  • Expansion headers supporting the 40-pin Pi-HAT compatible header, MikroE Click 16-pin header, and ADC/DAC 6-pin header
  • Audio applications are supported via onboard audio codec, digital microphone and stereo headphone jack I/O
  • Power is sourced via USB-C connector and is managed via the PCA9460B PMIC on the SOM, plus three additional voltage regulators

A unique aspect of this board is its debug subsystem which supports remote USB access to three UARTs, 16bit I/O expander-based remote control and monitoring, plus an option of using integrated SWD/JTAG or 10-pin header debugger interface. The built-in remote control, monitoring and integrated debugger are modeled on the capabilities on NXP’s i.MX 8ULP EVK platform, allowing developers to use NXP’s BCU software utility to remotely set boot mode, reset the board, reflash the memory and monitor the processor mode.

Expansion via a well-established ecosystem of HAT boards and Click boards (over 1,200 different MikroE Click boards are available) enables developers to tap into a broad range of prototyping options. An M.2 module connector on the backside of the carrier board facilitates easy addition of 801.11ac Wi-Fi and Bluetooth 5.1 connectivity using an optional certified M.2 wireless module. Other available accessories are a 7-inch MIPI-DSI LCD panel, a 5 MP MIPI-CSI camera and 5V/3A (USB-C connector) power supply.

For more information and the option to be notified on pricing and availability, please visit: http://avnet.me/MaaXBoard-8ULP.

 

About Avnet

As a leading global technology distributor and solutions provider, Avnet has served customers’ evolving needs for more than a century. We support customers at each stage of a product’s lifecycle, from idea to design and from prototype to production. Our unique position at the center of the technology value chain enables us to accelerate the design and supply stages of product development so customers can realize revenue faster. Decade after decade, Avnet helps its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com. 

 

Trademarks and brands are the property of their respective owners.

 

Avnet Media Contacts

Jeanne Forbis

Avnet

Jeanne.forbis@avnet.com

480-643-7499

 

Alex Jafarzadeh

Brodeur Partners, for Avnet

ajafarzadeh@brodeur.com

617-587-2846

Multimedia Files:

View all news