Evaluation boards for 2.5-40 GHz range digitally tunable filters and DC-40 GHz switches are available now
PHOENIX – Avnet (Nasdaq: AVT) is now shipping three ultra linear tunable RF filters and two wideband RF switches from Otava, a fabless mmW and mixed-signal IC design company best known for developing its OTBF103 millimeter wave beamformer IC. Both the filters and the switches are currently available as small form factor devices, which allows for maximum layout efficiency. Avnet is also offering Otava’s switch evaluation boards, which enable engineers to quickly assess the device’s performance and simplify prototyping and verification. To showcase the tunable RF filters in frequency-agile sub 6 GHz applications, Avnet is also developing a tunable filters daughter-card that will plug into a ZCU208 or ZCU216 Xilinx Zynq® UltraScale+™ RFSoC development board.
“Otava’s new tunable filters and mmW switches will provide designers with more high-performance solutions in the millimeter wave arena, where every component specification can make a difference in the overall system performance.” said Jim Beneke, vice president of Engineering and Technology, Avnet. “Their compact form factor, low insertion loss, and the wide band coverage allows for adoption in a range of systems including 5G and low Earth orbit (LEO) SATCOM applications.”
“We are extremely excited to announce that Otava’s ultra-wideband switches and tunable filters are now available through Avnet. They will serve as key components that are compatible with many existing platforms, including those in the 5G market,” said Otava Co-Founder and Vice President of Engineering, Wen Zheng. “The superior performance and flexibility of our products simplify architecture and reduce cost in many systems that are in need of refinement, especially in millimeter wave where the slightest enhancements matter.”
“Modern RF applications ranging from SDR and 5G to SATCOM, EW and more demand components with low insertion loss and small form factors,” says Mike Dunne, Precision RF Product Manager at Samtec. “The combination of Otava’s new low insertion loss RF filters and switches and Samtec’s Precision RF interconnect offers RF engineers and system designers high-performance components that optimize the entire RF signal path. Otava’s family of OTSW10x and OTFLx01 evaluation boards feature the latest Samtec 2.4 mm edge-mount compression connectors and launch optimizations.”
Tunable filters
Otava’s family of tunable filters covers multiple frequency bands for a range of different applications from 2.5 GHz to 40 GHz. These highly integrated tunable designs eliminate the need for multiple fixed frequency filters, which frees up valuable real estate for system implementation. The OTFL101 covers 2.5-7.5 GHz, the OTFL201 covers 14-24 GHz and the OTFL301 covers 24-40 GHz.
Each filter evaluation board consists of:
- one tunable filter
- two RF connectors
- a microcontroller
- an option for external control
The tunable filter evaluation boards OTFL101-EVAL, OTFL102-EVAL and OTFL103-EVAL are available for $1,495.00 (USD) each. Details and ordering links for the tunable filters and their evaluation boards can be found at: http://avnet.me/otava-filters
Switches
Otava’s single pole double throw (SPDT) switches offer exceptional insertion loss performance and linearity from DC to 40 GHz in a compact footprint. The OTSW100 is 2.546mm x 2.161mm, while the OTSW101 is 1.634mm x 1.637mm.
The switch evaluation boards offer a simple way to assess the device performance.
Each switch evaluation board consists of:
- the switch IC
- three 2.4mm connectors for the RFIO
- two +/- 2.5V control lines through a header
The switch evaluation boards OTSW100-EVAL and OTSW101-EVAL are available for $899.00 (USD) each. Details and ordering links for the switches and their evaluation boards can be found at: http://avnet.me/otava-switches.
About Otava, Inc.
Otava is a fabless mmW and mixed-signal IC design company founded in 2017 in Moorestown, N.J. Otava’s goal is to provide best-in-class wideband millimeter wave SoC components and turn-key system solutions in emerging wireless markets. Find out more about Otava at www.otavainc.com.
About Avnet
As a leading global technology distributor and solutions provider, Avnet has served customers’ evolving needs for an entire century. We support customers at each stage of a product’s lifecycle, from idea to design and from prototype to production. Our unique position at the center of the technology value chain enables us to accelerate the design and supply stages of product development so customers can realize revenue faster. Decade after decade, Avnet helps its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com.
Contacts:
Avnet Media Relations: Jeanne Forbis, jeanne.forbis@avnet.com, 480-643-7499
Brodeur Partners, for Avnet: Alex Jafarzadeh, ajafarzadeh@brodeur.com, 617-587-2846