Press Release Details

View all news

Avnet Launches XRF16-Gen 3 System-on-Module for Multi-Channel RF Applications

05/20/2021

New production-ready 16x16 direct-RF sampling module with 6 GHz analog bandwidth features the highly successful Xilinx UltraScale+ RFSoC Gen3 device

 

 

PHOENIX – May 20, 2021 The Avnet designed XRF16™ Xilinx RFSoC Gen 3 system-on-module (SoM) is now available for RF applications demanding small footprint, high-speed serial connectivity and real-time processing. Avnet (Nasdaq: AVT), the leading global technology solutions provider, is releasing the XRF16 module and Avalon™ software suite together to enable production-ready system development using the Xilinx Zynq® UltraScale+™ RFSoC Gen 3. The module is capable of RF direct conversion of signals with analog bandwidth up to 6 GHz. The release of the XRF16 Gen3 SOM doubles the channel density of the recently released XRF8 Gen3 SoM to address increasingly complex and demanding applications.

 

The Avnet XRF16 module can digitize 16 ADC channels at 2.5 giga-samples per second (GSPS) and generate complex (I/Q) waveforms through 16 DAC channels at 9.85 GSPS*. High-speed serial connectivity is available for 10/25/100 Gigabit Ethernet and Xilinx Aurora protocol. Baseband processing and network interface are handled by the Xilinx UltraScale+ RFSoC integrated quad Arm® Cortex®-A53 processing subsystem and programmable logic. Standard peripherals such as USB, Gigabit Ethernet and serial UART are included.

 

The XRF16 module allows users to begin prototype and application development immediately and then move to production quickly with the same hardware, which significantly reduces time to market. It is well-suited to support design work for radar, software-defined radio, beamforming, signal detection and jamming, and medical imaging applications.

 

“Developers require the latest, most advanced technology to deliver on their initiatives and projects,” said Jim Beneke, vice president of products and emerging technologies, Avnet. “Together with Xilinx, we created a production-ready module solution that frees developers to focus on the differentiating features of their products. This is our latest offering designed to accelerate time-to-market allowing developers to more quickly deliver real business value.”

 

“Combining high-speed digital and precision RF signals in a small form factor poses unique routing and isolation challenges,” said Mike Dunne, director of precision RF, Samtec. “The XRF16 module and companion carrier card leverage best-in-class RF and signal integrity design techniques to provide high-speed connectivity across the platform. System architects and designers can develop next-gen RF applications with confidence the XRF16 delivers the system performance needed.”

 

"The Zynq UltraScale+ RFSoC Gen-3 family includes new features, improves both DAC and ADC sample rates and extends the RF analog bandwidth of the 16T16R integrated multi-gigasample RF data converters for enhanced performance in demanding RF applications," said David Brubaker, Zynq UltraScale+ RFSoC product line manager, Xilinx. "Optimized for performance, size and power, the Avnet XRF16-Gen3 brings a drop-in solution to customers seeking fast-track integration of RFSoC Gen-3 technology into their products."

 

The Avnet XRF16 module is available for $24,995(USD). A companion carrier card is also available for $4,995 (USD). The products are available in the Americas and EMEA. Find more details about the kit at http://avnet.me/xrf16gen3-som.

 

* For operation up to 10 GSPS, contact your local Avnet sales team.

 

Follow Avnet on Twitter: @Avnet  

Follow Avnet on Instagram: http://www.instagram.com/Avnet

Connect with Avnet on Facebook: http://www.facebook.com/AvnetInc

Connect with Avnet on LinkedIn: http://www.linkedin.com/company/avnet

 

#Avnet, #Xilinx, #rfsoc, #samtec, #radar

 

All brands and trade names are trademarks or registered trademarks and are the properties of their respective owners. Avnet disclaims any proprietary interest in marks other than its own.

 

 

About Avnet
As a leading global technology distributor and solutions provider, Avnet has served customers’ evolving needs for an entire century. We support customers at each stage of a product’s lifecycle, from idea to design and from prototype to production. Our unique position at the center of the technology value chain enables us to accelerate the design and supply stages of product development so customers can realize revenue faster. Decade after decade, Avnet helps its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com.

 

 

Media Contacts

Jeanne Forbis

Avnet

jeanne.forbis@avnet.com

480-643-7499

 

Alex Jafarzadeh

Brodeur Partners, for Avnet

ajafarzadeh@brodeur.com

617-587-2846

 

Multimedia Files:

View all news