New development kit provides engineers with end-customer, certified LTE connectivity for IoT applications on Raspberry Pi HAT expansion-capable devices
PHOENIX--(BUSINESS WIRE)--
Leading global technology solutions provider Avnet (Nasdaq: AVT) today introduced the Monarch Go Pi HAT*, a new development kit to help product engineers and network developers enable simple, cost-effective LTE connectivity for IoT solutions. Utilizing the Monarch Go LTE-M modem component from Sequans (NYSE: SQNS), the new solution is ideal for use in business-critical applications, including asset tracking and remote monitoring.
With capabilities beyond a traditional cellular module, Monarch Go includes the LTE antenna and is pre-certified for end-customer use on the Verizon network, allowing engineers to significantly reduce lab testing and development time. Monarch Go is based on the Sequans Monarch GM01Q module that supports LTE-M and NB-IoT and is certified by leading operators in North America, Europe and Asia, giving it worldwide deployment and roaming capability. By combining Raspberry Pi HAT-capable single-board computers with Monarch Go, Avnet’s new Pi HAT offers lower cost of ownership and improved speed to market to develop a cellular IoT-connected device.
“Connectivity is the crucial pillar that all IoT solutions are built on, yet it presents one of the biggest hurdles for implementation,” said Jim Beneke, vice president of products and emerging technologies, Avnet. “By connecting Raspberry Pi HAT-compatible devices with Monarch Go LTE modems, developers and engineers can create seamless connectivity, saving time and money. This new component is the latest addition to Avnet’s end-to-end ecosystem of solutions and services to bring projects from idea to design, and design to production.”
“The Monarch Go Pi HAT development board is a boon to developers wanting to add LTE connectivity to their IoT devices,” said Nick Taluja, Sequans vice president of sales. “It makes it simple and easy to create and develop all kinds of IoT applications in a development environment that is widely used and understood, thus accelerating massive IoT deployment.”
The Monarch Go Pi HAT can operate in two modes for added development flexibility, either in conjunction with a single-board computer or in stand-alone mode, leveraging a micro USB interface. In addition, the Pi HAT includes a shuttle click expansion connector to enable 3.3V I/O I2C, SPI, UART and GPIO-based click modules from MikroElektronika. This expansion connector provides engineers with access to a large array of click module offerings, which can be used to prototype various LTE-based applications such as asset tracking, remote monitoring and embedded kiosks.
The Monarch Go Pi HAT kit includes a production-ready Monarch Go LTE modem with pre-installed ThingSpace IoT SIM, the MikroElektronika shuttle click site, voltage I/O translator and micro USB. Pi HAT supports both Monarch Go and Monarch Go-GPS modems.
The Monarch Go Pi HAT kit is available in the Americas for USD $72.95. Learn more about this product. Raspberry Pi products and accessories, including the new Raspberry Pi 4 Model B computer with 8GB of onboard memory, are available from Newark, an Avnet Company.
*HAT stands for “hardware attached on top,” a hardware specification for add-on modules compatible with all Raspberry Pi models from B+ onwards. HATs have several advantages compared to older add-on modules for the Raspberry Pi, such as no soldering required — just plug it onto the Raspberry Pi.
About Avnet
Avnet is a global technology solutions provider with an extensive ecosystem delivering design, product, marketing and supply chain expertise for customers at every stage of the product lifecycle. We transform ideas into intelligent solutions, reducing the time, cost and complexities of bringing products to market. For nearly a century, Avnet has helped its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com. (AVT)
View source version on businesswire.com:
https://www.businesswire.com/news/home/20200825005307/en/
Avnet Media Relations:
Jeanne Forbis; jeanne.forbis@avnet.com; 480-643-7499
Brodeur Partners, for Avnet:
Alex Jafarzadeh; ajafarzadeh@brodeur.com; 617-587-2846
Source: Avnet