Allows design and system engineers to develop embedded vision applications with camera sensor modules at a much lower cost of entry
PHOENIX--(BUSINESS WIRE)--
Leading global technology solutions provider Avnet (Nasdaq: AVT) today introduced the 96Boards ON Semiconductor Dual Camera Mezzanine development and prototyping platform for the AP1302 imaging processor coupled with dual imaging camera modules. This platform will enable design and system engineers to create cost-effective embedded vision applications utilizing industry-standard technologies.
The two Imager Access System (IAS) camera modules that ship standard on this Mezzanine use the AR0144 monochrome digital image sensor from ON Semiconductor. The AR0144 is a 1-megapixel Mobile Industry Processor Interface (MIPI) sensor (1280 horizontal by 800 vertical resolution) and will run at 60 frames per second at full resolution. Its innovative global shutter pixel design is optimized for accurate and fast capture of moving scenes while producing clear, sharp digital images. The ability to capture clear images is critical for applications such as scanning, industrial inspection and drone navigation.
By using the 96Boards standard, this card can easily enable low-latency vision system prototyping by leveraging the many capabilities of the Xilinx Ultra96-V2 platform.
“This prototyping platform is specially created for design engineers, system engineers and suppliers to focus on IoT vision, AI and computer imaging applications,” said Jim Beneke, vice president of products and emerging technologies, Avnet. “It simplifies the complex process of developing applications with imaging sensors. In addition, Avnet has matched this card with our Ultra96-V2 to provide a very high performance, cost-effective AI vision platform.”
The platform utilizes MIPI and the camera serial interface (CSI2) standardizations which are specifications of the MIPI Alliance. The MIPI-CSI2 specification defines the interface between the image sensors, ISP and a host processor, and is widely used for high-speed communications output from image sensors in most embedded systems.
The API 1302 image co-processor from ON Semiconductor performs image processing functions within the platform, including turning, configuration and calibration of the sensors. These processing functions also help to reduce design efforts of developing an embedded camera system. The AP1302 interfaces the sensors and the host processor using MIPI-CSI2 lanes.
The IAS image sensor module interface from ON Semiconductor helps solve this problem and enables:
1) Simplified camera system design: A single, standardized interface helps to quickly connect the imaging module to the processing board, such as the 96Boards Mezzanine.
2) Shorter lifecycle: Solution decreases time to market by enabling low-touch design.
3) Lowered learning curve: Prior imaging system expertise is not required since IAS is a plug-and-play solution.
The purpose of the standardized IAS interface is to help any embedded vision system or board designer to gain access to all compatible image sensor modules.
“By combining the readily available ON Semiconductor image sensor-based IAS modules with the capability and flexibility of the AP1302 ISP, we have enabled manufacturers to easily prototype designs using the industry-standard 96Boards format,” said Gianluca Colli, vice president and general manager, Consumer Solutions Division of the Intelligent Solutions Group at ON Semiconductor.
The Avnet-designed 96Boards ON Semiconductor Dual Camera Mezzanine development and prototyping platform comes with two IAS sensor modules and an AP1302 imaging co-processor. It is available today in the Americas, EMEA, APAC and Japan for $199 (USD). Learn more about the kit.
About ON Semiconductor
ON Semiconductor (Nasdaq: ON) is driving energy efficient innovations, empowering customers to reduce global energy use. The company is a leading supplier of semiconductor-based solutions, offering a comprehensive portfolio of energy efficient, power management, analog, sensors, logic, timing, connectivity, discrete, SoC and custom devices. The company’s products help engineers solve their unique design challenges in automotive, communications, computing, consumer, industrial, medical, aerospace and defense applications. ON Semiconductor operates a responsive, reliable, world-class supply chain and quality program, a robust compliance and ethics program, and a network of manufacturing facilities, sales offices and design centers in key markets throughout North America, Europe and the Asia Pacific regions. For more information, visit http://www.onsemi.com. Follow @onsemi on Twitter.
About Avnet
Avnet is a global technology solutions provider with an extensive ecosystem delivering design, product, marketing and supply chain expertise for customers at every stage of the product lifecycle. We transform ideas into intelligent solutions, reducing the time, cost and complexities of bringing products to market. For nearly a century, Avnet has helped its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com.
Follow Avnet on Twitter: @Avnet
Follow Avnet on Instagram: http://www.instagram.com/Avnet
Connect with Avnet on Facebook: http://www.facebook.com/AvnetInc
Connect with Avnet on LinkedIn: http://www.linkedin.com/company/avnet
All brands and trade names are trademarks or registered trademarks, and are the properties of their respective owners. Avnet disclaims any proprietary interest in marks other than its own.
View source version on businesswire.com:
https://www.businesswire.com/news/home/20200910005365/en/
Avnet Media Relations:
Jeanne Forbis, jeanne.forbis@avnet.com, 480-643-7499
Brodeur Partners, for Avnet:
Alex Jafarzadeh, ajafarzadeh@brodeur.com, 617-587-2846
Source: Avnet