Press Release Details

View all news

Avnet Introduces Cost-Optimized MiniZed Platform for Embedded Vision and Industrial IoT Systems

06/13/2017

Single-Core Zynq-7000 SoC-based board delivers performance in small form factor for entry-level application development

Avnet (NYSE: AVT), a leading global technology distributor, today introduced the compact and cost-effective MiniZed Zynq SoC development platform. MiniZed provides an entry-level development and demonstration platform for single-core Xilinx® Zynq®-7000 All Programmable SoC devices. This cost-optimized solution supports cloud connectivity and industrial IoT applications such as motor control and embedded vision. The $89 starter kit is now available for ordering, with shipments starting in early July. A video demonstration of the MiniZed technology can be viewed here.

Showcasing the power of the Zynq-7000S SoC device family, which features a single-core ARM® Cortex-A9 processor paired with 28nm Artix®-7 based programmable logic, MiniZed represents the lowest cost entry point to the scalable Xilinx Zynq-7000 All Programmable SoC development platform. MiniZed’s compact design – small enough to fit into a shirt pocket – features on-board connectivity through USB, Wi-Fi and Bluetooth. Peripherals can be plugged into dual Pmod-compatible connectors, the Arduino-compatible shield interface or the USB 2.0 host interface. User LEDs, a button and a switch allow for a physical board interface, while JTAG circuitry is incorporated onto the MiniZed base board. Tutorials, which will be available for download at http://minized.org, use the on-board microphone as an example input to demonstrate how to easily implement filters and FFTs in the fabric. The on-board eMMC (8GB) provides convenient storage for the OS, files and logs.

“Whether customers are developing a Linux-based system or have a simple bare metal implementation, with MiniZed, Zynq-7000 development has never been easier,” said Stefan Rousseau, senior technical marketing engineer for Avnet. “Designers need only connect to their laptops with a single micro-USB cable and they are up and running. And with Bluetooth or Wi-Fi, users can also connect wirelessly, transforming a mobile phone or tablet into an on-the-go GUI.”

“Avnet's new MiniZed offers customers a low-cost entry point to high performance Zynq-7000 single-core ARM Cortex-A9 based SoC devices,” said Evan Leal, director of product marketing at Xilinx. “The kit is designed for ease of use with tutorials that accelerate customer prototyping for embedded designs. MiniZed also features Xilinx’s SDSoC™ Development Environment, which enables software engineers to quickly migrate compute-intensive C/C++ functions to hardware, effectively accelerating the functions and offloading the processor.”

The MiniZed platform is supported by the minized.org community website, where users can collaborate with other engineers also working on Zynq designs. Click here for more information and to place your order.

Click to Tweet: New #MiniZed #Zynq platform from @Avnet jump-starts #IIOT development with @XilinxInc single-core #Zynq-7000 SoCs http://bit.ly/1ll33LR

Follow Avnet on Twitter: @Avnet
Connect with Avnet on LinkedIn: http://www.linkedin.com/company/avnet
Connect with Avnet on Facebook: http://www.facebook.com/AvnetInc

All brands and trade names are trademarks or registered trademarks, and are the properties of their respective owners. Avnet disclaims any proprietary interest in marks other than its own.

About Avnet

From idea to design and from prototype to production, Avnet supports customers at each stage of a product’s lifecycle. A comprehensive portfolio of design and supply chain services makes Avnet the go-to guide for innovators who set the pace for technological change. For nearly a century, Avnet has helped its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com.

Avnet
Maureen O’Leary, 480-643-7499
maureen.oleary@avnet.com
or
Brodeur Partners
Jamie Ernst, 480-308-0286
jernst@brodeur.com

Multimedia Files:

View all news