PHOENIX--(BUSINESS WIRE)--Avnet,
Inc. (NYSE: AVT),
a leading global technology distributor, today released the PicoZed™
Software-Defined Radio SDR 1x1, a rugged, low-power, system-on-module
(SOM). Priced at $549, the PicoZed SDR 1x1 is cost optimized for
single-channel transmit and receive signal paths in the 70 MHz to 6.0
GHz range, and is available to customers in the Americas, EMEA, Asia and
Japan.
The full-duplex PicoZed SDR 1x1 combines the AD9364 integrated RF Agile
Transceiver™ from Analog Devices, Inc. with a Xilinx® Zynq®-7020 All
Programmable SoC, and features the same handheld form-factor as Avnet’s
dual-channel PicoZed
SDR 2x2. By integrating the critical RF signal path and high-speed
programmable logic in a fully verified SOM, the PicoZed SDR 1x1 enables
designers to dramatically reduce cycle times for the development of the
RF-to-baseband signal processing core in wireless communications systems
for markets, including defense/aerospace, security/surveillance,
portable systems and 3G/4G communications.
The PicoZed SDR 1x1 SOM is supported by robust simulation and code
generation tools that integrate seamlessly with Xilinx Vivado®
Design Suite. For fast prototyping of software-defined radio products,
PicoZed SDR 1x1 is compatible with the PicoZed SDR FMC Carrier Card
(AES-PZSDRCC-FMC-G), providing standard high bandwidth interfaces like
USB, Gigabit Ethernet and RF power modules. Fast data streaming to
MATLAB and Simulink from MathWorks is supported to speed algorithm
development and aid in the verification of system designs.
“Next-generation wireless systems across all market segments, from 3G/4G
small cells to military and industrial, will be driven by imperatives of
size, power and cost reduction. Software-defined radio technology
provides designers of portable communications devices with flexibility
and upgradability that far surpass the limits of traditional
hardware-only customization,” said Luc Langlois, director, global
technical marketing, Avnet Electronics Marketing. “Designed for
immediate prototype and quick integration in customers’ end application,
the PicoZed SDR 1x1 reduces the cost, risk, and time required to develop
and deploy production-ready SDR systems.”
“PicoZed SDR 1x1 extends the PicoZed SDR family with a single-channel
solution based on the AD9364 RF Agile Transceiver,” said Robin Getz,
director of engineering, Analog Devices. “For software developers
targeting the dual ARM Cortex A9 within the Zynq SoC, PicoZed SDR 1x1 is
supported through libiio, a comprehensive API with C, C++, C# and Python
bindings. The various carriers provide a multitude of connectivity, from
Dual Gigabit Ethernet to USB, allowing live data streaming into various
SDR design environments, including MATLAB/Simulink. SDR developers can
now quickly move from algorithm development to cost-optimized product,
using the same radio and base band processor hardware.”
To help wireless system designers maximize the performance potential of
the PicoZed SDR SOMs, Avnet offers a series of online software-defined
radio SpeedWay Design Workshops™, created in collaboration with Analog
Devices, MathWorks and Xilinx. The pre-recorded SpeedWay course modules
demonstrate hands-on design techniques with system-level reference
designs to deploy SDR systems using the PicoZed SDR. Further information
about the online SpeedWay Design Workshops can be found at
https://products.avnet.com/wps/portal/ema/event/software-defined-radio-picozed-sdr-speedway-workshop-2015/
.
The PicoZed SDR 1x1 system-on-module (SOM) is available for order today
from Avnet. Further information on the PicoZed SDR SOMs and Carrier
Cards can be found at http://picozed.org/.
Click
to Tweet: .@Avnet reduces cost, risk and development time for
production-ready SDR systems with new #PicoZed SDR 1x1 http://bit.ly/1ll33LR
Follow Avnet on Twitter: @Avnet
Connect
with Avnet on LinkedIn: http://www.linkedin.com/company/avnet
Connect
with Avnet on Facebook: http://www.facebook.com/AvnetInc
About Avnet, Inc.
From components to cloud and design to disposal, Avnet, Inc. (NYSE:AVT)
accelerates the success of customers who build, sell and use technology
globally by providing them with a comprehensive portfolio of innovative
products, services and solutions. For more information, visit www.avnet.com.
MATLAB and Simulink are registered trademarks of The MathWorks, Inc.
See
mathworks.com/trademarks
for
a list of additional trademarks. Other product or brand names may be
trademarks or registered trademarks of their respective holders.
Avnet, Inc.
Maureen O’Leary, 480-794-6152
Director, Media Relations
Maureen.OLeary@avnet.com