Avnet,
Inc. (NYSE: AVT),
a leading global technology distributor, released the PicoZed™ FMC
Carrier Card V2, a next-generation platform with improved FPGA Mezzanine
Card (FMC) interface, transceiver signal integrity and clocking, all at
a more cost-competitive price point. Engineers can view a video
previewing the kit’s key features here.
The new FMC carrier card kit speeds prototyping and development of Xilinx®
Zynq®-7000 All Programmable SoC systems based on the
PicoZed family of System-on-Modules (SOMs). The carrier enables many key
interfaces for the on-module Gigabit Ethernet PHY and USB PHY, including
a bootable microSD card slot and USB-UART port. A majority of the
PicoZed’s programmable logic I/O are made available through a Low-Pin
Count (LPC) FMC connector, which accommodates many available add-on
cards including industrial Ethernet, video/camera I/O, motor control,
software-defined radio or quad gigabit Ethernet.
In addition, the carrier features an HDMI output port, real-time clock,
high-performance clock synthesizer, two MAC ID EEPROMs and several
Digilent-compatible Pmod™ ports. The four serial transceivers on the
PicoZed 7015 and 7030 SOMs are allocated to a x1 PCIe Gen2 card edge
interface, the FMC connector, an SFP+ interface and general purpose SMA
connectors.
The PicoZed FMC Carrier Card V2 Kit ships with a microSD card pre-loaded
with a custom-configured Pulsar™ Linux operating system from Wind River®,
a global leader in delivering software for the Internet of Things (IoT).
This allows designers to begin application development right out of the
box.
“The PicoZed SOM enables embedded systems designers to more quickly and
cost-effectively leverage the industry-leading integration, performance,
power and security of the Zynq-7000 All Programmable SoCs,” said Bryan
Fletcher, technical marketing director, Avnet. “Now, the new PicoZed FMC
Carrier Card V2 will further accelerate Zynq product development by
providing a platform for immediate prototyping and a reference PCB
design to use as a starting point for a custom carrier.”
The PicoZed FMC Carrier Card V2 Kit includes:
-
PicoZed FMC Carrier Card V2
-
8 GB microSD card preloaded with Wind River Pulsar™ Linux (with SD
adapter card)
-
USB A-to-microB cable
-
ATX-to-6P Mini-Fit adapter
-
PCIe bracket
-
Mounting hardware for SOM
-
12V AC/DC international supply
-
Quick Start instructions for the board and Pulsar
The new PicoZed FMC Carrier Card V2 Kit, priced at $349, is currently
available for ordering. Please visit http://picozed.org
for more information.
Click
to Tweet: PicoZed FMC Carrier Card from @avnetdesignwire improves
FMC interface, transceiver signal integrity and clocking http://bit.ly/1ll33LR
Connect with Avnet:
Connect
with us on social media
Contribute
to our technical forums
View product and company
videos
Buy
our components
About Avnet, Inc.
From components to cloud and design to disposal, Avnet, Inc. (NYSE:AVT)
accelerates the success of customers who build, sell and use technology
globally by providing them with a comprehensive portfolio of innovative
products, services and solutions. Avnet is a Fortune 500 company with
revenues of $27.9 billion for the fiscal year 2015. For more
information, visit www.avnet.com.

Avnet Electronics Marketing
Heidi Elliott, 480-643-7584
Senior Director, Marketing Programs
Heidi.Elliott@avnet.com