Press Release Details

View all news

Avnet Electronics Marketing Introduces the Spartan®-6 FPGA Motor Control Development Kit

12/13/2011

PHOENIX--(BUSINESS WIRE)--Avnet Electronics Marketing, an operating group of Avnet, Inc. (NYSE: AVT), announced today the launch of their latest development platform for designers implementing motor control systems, the Spartan®-6 FPGA Motor Control Development Kit. Designed in collaboration with Xilinx, Inc., the Spartan-6 FPGA Motor Control Development Kit enables engineers to prototype motor control designs for applications in industrial automation, consumer electronics, medical diagnostics and robotics. For more details, or to place an order, visit the Spartan-6 FPGA Motor Control Development Kit information page on AvnetExpress.com.

The Spartan-6 FPGA Motor Control Development Kit is an ideal platform for designers seeking to experiment with proven reference designs and develop custom control, integrating flexible peripheral functions like Ethernet, PowerLink and PCI Express (PCIe). Other features of the kit include:

  • Avnet’s Xilinx Spartan-6 LX75T FPGA base board with PCIe edge connector, 10/100 Ethernet PHY, and dual 128MB DDR3 SDRAM banks;
  • Avnet Motor Control FPGA Mezzanine Adapter (FMC) module;
  • One Portescap Brushless DC (BLDC) motor with Hall Effect sensor;
  • One Portescap stepper can stack motor; and
  • One 12 V power supply and adapter cable.

The Avnet Motor Control FMC module features the Low Pin Count (LPC) form factor enabling attachment to any Avnet or Xilinx FMC-enabled platform. Each Avnet Motor Control FMC can drive one Stepper motor, two Brushed DC (BDC), two BLDC, or two Permanent Magnet Synchronous Motors (PMSM). Other features include:

  • DRV8312 integrated, three-phase, fractional-horsepower motor driver from Texas Instruments (TI) for high-current output;
  • Quad ADS1204 integrated delta-sigma modulator from TI for high-precision sensing;
  • Xilinx XADC header enabling low-cost 7 series FPGA integration;
  • Hall sensor/Encoder and General Purpose Input/Output (GPIO) ports;
  • Drive stage voltage range from 12-24 V with external power option; and
  • A user prototype area for custom hardware modifications.

“Working closely with Xilinx engineers, Avnet’s technical team created a kit that is both versatile and easy to use for designers looking to develop and verify motor control algorithms,” said Jim Beneke, vice president of global technical marketing, Avnet Electronics Marketing. “At its core, this kit utilized the Xilinx Spartan-6 FPGA, which enables a motor control performance advantage over standard microcontroller or DSP implementations, while also offering a unique integration capability that only an FPGA-based solution can offer.”

“By building their motor control systems using Spartan-6 FPGAs, developers can lower their total cost of ownership by conserving power through tighter control of speed, torque and acceleration, while improved efficiency allows for smaller, less expensive motors,” said Harry Raftopoulos, director of Xilinx's Industrial Business Segment. “The Spartan-6 FPGA Motor Control Development Kit gives these developers a comprehensive and scalable development platform for building these applications easily.”

“Selecting the right motor driver is critical to the design of any high-performance, motorized application,” said Marc Royer, marketing manager for TI’s Precision Data Converter and Motor Drive businesses. “The DRV8312 motor driver, combined with the ADS1204 delta sigma modulator, enable Avnet to provide high-performance, high-precision and power-efficient motor control that is also robust, reliable and fully protected.”

“Portescap’s compact, high-precision, high power BLDC and stepper motors are the perfect complement to Avnet’s Motor Control FMC module,” said William Anderson, director of international sales at Portescap. “The combination of Portescap and Avnet provide a complete motor control solution for our combined customers.”

For more information, or to order the Avnet Spartan®-6 FMC Development Kit, visit www.em.avnet.com/spartan6motor.

Additional Resources

Avnet and Xilinx will host a live webcast during Q1 2012, to demonstrate some of the features of this new kit. For details visit www.em.avnet.com/spartan6motor.

Connect with Avnet

Follow Avnet on Twitter

Contribute to our technical forums

View product and company videos

Buy our components

About Avnet Electronics Marketing

Avnet Electronics Marketing is an operating group of Phoenix-based Avnet, Inc. that serves electronic original equipment manufacturers (EOEMs) and electronic manufacturing services (EMS) providers in more than 70 countries, distributing electronic components from leading manufacturers and providing associated design-chain and supply-chain services. The group's website is located at www.em.avnet.com.

About Avnet, Inc.

Avnet, Inc. (NYSE: AVT), a Fortune 500 company, is one of the largest distributors of electronic components, computer products and embedded technology serving customers in more than 70 countries worldwide. Avnet accelerates its partners' success by connecting the world's leading technology suppliers with a broad base of more than 100,000 customers by providing cost-effective, value-added services and solutions. For the fiscal year ended July 3, 2010, Avnet generated revenue of $19.16 billion. For more information, visit www.avnet.com.

Photos/Multimedia Gallery Available: http://www.businesswire.com/cgi-bin/mmg.cgi?eid=50104028&lang=en

Avnet Electronics Marketing
Bethany Helvie, 480-643-7183
Public Relations
Bethany.Helvie@avnet.com

Multimedia Files:

Avnet introduces the Spartan-6 FPGA Motor Control Development Kit. (Photo: Business Wire) 2788 x 1324 jpg 3.36 MB
View all news