Newsroom

Security Comes Full Circle: Avnet Advances IoT Security with Azure Sphere Starter Kit

New kit accelerates rapid prototyping by giving developers easy access to the fastest and easiest way to equip IoT endpoint devices to be highly secure

Category:

Monday, January 7, 2019 8:00 am MST

Dateline:

PHOENIX

Public Company Information:

NASDAQ:
AVT

.@Avnet #AzureSphere Starter Kit is the fastest and easiest way to equip #IoT endpoint devices to be highly #secure, ensuring that developers can quickly move from prototype to production. #CES2019 Visit Avnet booth 2609 to learn more.

PHOENIX--(BUSINESS WIRE)--Security is the biggest challenge to developers bringing new IoT endpoint devices to market. To meet this need, leading global technology solutions provider, Avnet (Nasdaq: AVT) today introduced the Avnet Azure Sphere MT3620 Starter Kit, which supports rapid prototyping of IoT implementations using Microsoft’s Azure Sphere, an end-to-end solution for creating highly-secured, connected Microcontroller (MCU) devices. Avnet will demonstrate the new starter kit for the first time at CES 2019, in booth #2609 at Tech East, Westgate Las Vegas Resort.

The Starter Kit leverages the Avnet-developed Azure Sphere module that is based on the MT3620 reference development board. The production-ready module is the fastest and easiest way to equip IoT endpoint devices to be highly secure, ensuring that developers can quickly move from prototype to production.

Last spring, Microsoft named Avnet as a strategic partner for Azure Sphere and the first to distribute the solution. Today’s introduction of the Avnet Azure Sphere MT3620 Starter Kit further helps developers accelerate their IoT deployments while also addressing security holistically, from the silicon layer to the cloud. The kit is ideal for creating secured IoT edge devices, such as consumer appliances, as well as smart retail, remote access, building and factory automation applications.

In a recent survey of the Hackster.io and element14 engineering communities, Avnet found that developers believe security remains the biggest technological hurdle in IoT deployment (81 percent).

“Security is critical to continued growth within the connected devices market,” said Jim Beneke, vice president, engineering and technology, Avnet. “Microsoft has delivered significant advancements in connected security with Azure Sphere. Our new starter kit builds on that by offering an easy way for customers to accelerate prototyping, proof-of-concept development and time to market of their Azure Sphere powered devices, while providing confidence in the security of their solutions.”

The Avnet Azure Sphere MT3620 Starter Kit includes a small form factor carrier board supporting Avnet’s production ready Azure Sphere MT3620 module with WiFi connectivity. Multiple expansion interfaces provide developers with easy integration of off-the-shelf sensors, displays, motors, relays and more. The downloadable “getting started” tutorial guides developers through the development steps from board setup to application coding.

“Avnet is pushing to accelerate the adoption of secure, connected MCU solutions with Azure Sphere,” said Rodney Clark, vice president IoT, Microsoft. “The Avnet Azure Sphere MT3620 Starter Kit provides developers with the components, tools and resources they need to efficiently build and bring a wide variety of innovative and highly secured MCU devices and solutions to market.”

The Avnet Azure Sphere MT3620 Starter Kit is now available to pre-order for $75 USD, with delivery scheduled for early April. More information about this starter kit is available at: http://avnet.me/mt3620-kit.

Technical Specifications:

Carrier board features include:

  • Two MikroE Click Board expansion sockets
  • Grove expansion connector (I2C)
  • On-board sensors
    • 3-Axis accelerometer
    • 3-Axis gyro
    • Temperature
    • Pressure/Barometric
  • Interface for optional OLED 128x64 display
  • USB Interface
    • Supports debug, service and recovery UARTs, and JTAG
  • User push switches and LEDs
  • 5V to 3.3V Power regulation
  • DC Supply Input:
    • USB 5V from host computer
    • Terminal foot prints for external 5VDC and VBAT supplies

Azure Sphere MT3620 Module features include:

  • 3x ISU interfaces pre-configured for UART, SPI, I2C
  • ADC/GPIO: 3x 12-bit ADC inputs (or 3 GPIOs)
  • PWM/GPIO: 9x PWM outputs (or up to 24 GPIOs)
  • RTC (requires VBAT supply)
  • Dual-band 2.4/5GHz 802.11 a/b/g/n WiFi
  • Dual-band 2.4/5GHz chip antenna
  • Production-ready

Follow Avnet on Twitter: @Avnet
Follow Avnet on Instagram: https://www.instagram.com/Avnet/
Connect with Avnet on Facebook: http://www.facebook.com/AvnetInc
Connect with Avnet on LinkedIn: http://www.linkedin.com/company/avnet

All brands and trade names are trademarks or registered trademarks, and are the properties of their respective owners. Avnet disclaims any proprietary interest in marks other than its own.

About Avnet

Avnet is a global technology solutions provider with an extensive ecosystem delivering design, product, marketing and supply chain expertise for customers at every stage of the product lifecycle. We transform ideas into intelligent solutions, reducing the time, cost and complexities of bringing products to market. For nearly a century, Avnet has helped its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com.

Contact:

Media Relations Contacts
Maureen O’Leary
Maureen.OLeary@avnet.com
480-643-7499

Jamie Ernst
Brodeur Partners, for Avnet
jernst@brodeur.com
480-308-0286

Multimedia Files:

Preview image
Avnet introduces the Azure Sphere MT3620 Starter Kit, which supports rapid prototyping of IoT implementations using Microsoft’s Azure Sphere. Avnet will demonstrate its new starter kit for the first time at CES 2019, booth #2609 at Tech East, Westgate Las Vegas. (Photo: Business Wire)
Preview image

$Cashtags