Newsroom

Avnet Releases Low-Cost Gigabit Network FMC Module

Utilizing Ethernet PHYs from Microchip, new module accelerates development of Industrial IoT

Category:

Tuesday, September 11, 2018 8:00 am MST

Dateline:

PHOENIX

Public Company Information:

NASDAQ:
AVT

.@Avnet announces new #Network FMC Module that offers designers of #industrial #IoT Gigabit Ethernet switching at less than half the cost of other devices.

PHOENIX--(BUSINESS WIRE)--Avnet (Nasdaq: AVT), a leading global technology solutions provider, today introduced the Avnet Network FMC Module, offering designers of emerging industrial Internet of Things (IoT) applications industry-leading Gigabit Ethernet switching at less than half the cost of devices currently available on the market. Optimized for Xilinx FPGA and SoC-based industrial Ethernet digital communications systems, the new Dual 1000 Mbps Networking FMC Module supports applications such as cloud-based data centers and industrial automation.

“By bringing together key technologies from Microchip, Avnet and Xilinx, we have succeeded in developing a Network FMC Module that satisfies customer needs for gigabit Ethernet, while dramatically reducing the cost to deploy,” said Kevin Keryk, technical marketing manager, Avnet. “This Network FMC Module opens up a world of possibilities for designers to accelerate development of industrial IoT and connected factory systems, including Gigabit Ethernet switches, industrial IoT gateways, hardware-accelerated routers and real-time Time-Sensitive Networking (TSN).”

This versatile new module has several reference designs that are compatible with Avnet’s own UltraZed family of boards, plus this VITA 57 standards-based module is also compatible with other Xilinx Zynq-UltraScale+ boards available on the market today.

Technical Specifications:

  • FMC LPC single-width module
  • Dual RGMII 10/100/1000 Ethernet PHY
  • Dual Ethernet MAC ID EEPROM
  • IPMI EEPROM
  • Bi-Color Status LEDs
  • 3.3V - 1.8V IO Voltage compatibility

Now available to customers in the Americas, EMEA, Asia and Japan, the Network FMC module (AES-FMC-NETW1-G) is priced at $149. For more information, visit http://avnet.me/fmc-network1. Reference designs using the recommended equipment can be found on the Reference Design Page for the UltraZed-EG + PCIe Carrier Card. Additional reference material is available on the Network FMC accessory page, http://avnet.me/fmc-network1-doc.

Follow Avnet on Twitter: @Avnet
Connect with Avnet on LinkedIn: http://www.linkedin.com/company/avnet
Connect with Avnet on Facebook: http://www.facebook.com/AvnetInc

All brands and trade names are trademarks or registered trademarks, and are the properties of their respective owners. Avnet disclaims any proprietary interest in marks other than its own.

About Avnet

From idea to design and from prototype to production, Avnet supports customers at each stage of a product’s lifecycle. A comprehensive portfolio of design and supply chain services makes Avnet the go-to guide for innovators who set the pace for technological change. For nearly a century, Avnet has helped its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com.

Contact:

Avnet
Maureen O’Leary
maureen.oleary@avnet.com
480-643-7499
or
Brodeur Partners for Avnet
Jamie Ernst
jernst@brodeur.com
480-308-0286

Multimedia Files:

Preview image
The new Network FMC Module from Avnet offers designers of industrial IoT applications industry-leading Gigabit Ethernet switching at less than half the cost. (Photo: Business Wire)
Preview image

$Cashtags