Newsroom

Avnet Electronics Marketing Introduces the Freescale Semiconductor MPC885 PowerQUICC Evaluation Kit

Monday, October 11, 2004 2:29 pm MST

Dateline:

PHOENIX

Public Company Information:

NYSE:
AVT
"We are pleased to work with Avnet to bring this flexible and integrated suite to this market segment."
PHOENIX--(BUSINESS WIRE)--Oct. 11, 2004--Avnet Electronics Marketing announces a new evaluation kit featuring an integrated platform to develop and test designs featuring the highly advanced Freescale Semiconductor MPC885 PowerQUICC(TM) Integrated Communications Processor. The kit features 10/100 Ethernet, USB and RS-232 console interfaces to transport processed data via an AvBus parallel interface from a host system. A complete software development suite including a Linux board support package is included with the kit for maximum design flexibility. The kit also includes a complete bill of materials and schematics.

"Avnet Electronics Marketing is committed to delivering tools that enable our suppliers to bring new technology to our customers more efficiently," explained Jim Schaeffer, senior VP of Avnet Design Services. "This Avnet kit was developed to simplify and shorten the often complicated communication design process and provide the necessary hardware and software to give developers a quick start in their next design."

"The reference kit developed by Avnet is a valuable tool for our mutual customers to test drive Freescale's MPC885 processor in a variety of communications applications," continued Mike Shoemake, PowerQUICC marketing manager at Freescale Semiconductor. "We are pleased to work with Avnet to bring this flexible and integrated suite to this market segment."

The MPC885 PowerQUICC processor offers an integrated security engine, dual Fast Ethernet interfaces, and USB support (full/low-speed) in a low-cost communications processor architecture. The family supports core frequencies scaling from 66 MHz to 133 MHz and external bus speeds of up to 80 MHz. Like all PowerQUICC processors, the MPC885 family devices integrate two processing blocks: an embedded 8xx PowerPC core (with an 8 KB instruction cache and an 8 KB data cache) and an on-chip Communications Processor Module (CPM).

The MPC885 excels in communication, networking and industrial control systems, demonstrating the enhanced benefits of a leading-edge network controller solution. A variety of memory technologies are implemented to allow full utilization of the MPC885 controller functions.

The Freescale Semiconductor MPC885 Evaluation Kit is available for purchase today. Contact your local Avnet Electronics Marketing sales office or visit the Web at www.em.avnet.com/MPC885 for more information. Ordering part number and price is:

  ADS-FRS-885-EVL               $499 USD 

The MPC885 Evaluation Kit includes the following features:

-- Freescale's MPC885 PowerQUICC(TM) I Processor (133 MHz) with integrated security engine

-- AvBus expansion connectors

-- 64 MB SDRAM

-- 16 MB FLASH

-- 1 MB SRAM

-- RS-232 console port

-- USB 2.0 low/full-speed port (host or endpoint)

-- Dual 10/100 Mbps Ethernet port

-- Linux Board Support Package

About Avnet Electronics Marketing

Avnet Electronics Marketing, serving customers in 68 countries, is the largest operating group of Phoenix-based Avnet Inc. (NYSE:AVT), a Fortune 500 company with fiscal 2004 sales of over $10 billion, and one of the world's largest technology marketing, distribution and services companies. Avnet Electronics Marketing, Americas (EMA) serves electronic original equipment manufacturers (EOEMs) and electronic manufacturing services (EMS) providers in North America and Brazil distributing electronic components from leading manufacturers and providing associated services. The company's Web site is located at www.em.avnet.com.

Contact:

Avnet Electronics Marketing
Jennifer Read, 480-643-2931
Jennifer.read@avnet.com