Avnet now offers the Advantech MIO-5355, a compact Arm-based single-board computer designed to deliver high-performance AI processing in space-constrained and power-sensitive environments. Built on Qualcomm’s QCS6490 and QCS5430 SoCs, the MIO-5355 provides up to 12.3 TOPS of AI acceleration, enabling real-time edge inference for demanding industrial and embedded applications.
The MIO-5355 combines advanced AI performance with low power consumption, making it ideal for smart manufacturing, robotics, surveillance and edge computing. By processing data locally, it reduces reliance on cloud infrastructure, minimizing latency, enhancing security and improving system responsiveness.
Featuring an 8-core Arm processor, LPDDR5 memory and versatile connectivity options such as ethernet, USB and M.2 slots for Wi-Fi or 5G expansion, the MIO-5355 delivers robust performance in a compact 3.5-inch form factor. Its design supports continuous 24/7 operation across wide temperature ranges, essential for dependable performance in industrial environments.
Advantech developed the MIO-5355 with complete hardware and software integration, including board support packages for Windows on Arm and Ubuntu Linux. The company also provides customization, scalability and global technical support to help OEMs and system integrators accelerate deployment of AI-driven solutions across multiple verticals, from smart cities to factory automation.
The Advantech MIO-5355 brings powerful, energy-efficient AI capabilities directly to the edge, helping customers build faster, smarter and more reliable connected systems.
For more information on the MIO-5355, visit https://www.avnet.com/americas/manufacturers/m/advantech/.